Other Parts Discussed in Thread: BQSTUDIO
Hi
终端客户的问题是:用的BQ40Z50-R1的IC,启动了shipmode这个功能,设置的时间是64800,大部分电池都会自动进入,但是有小部分没有进入,需要找这个原因,还请帮忙协助分析,谢谢。
附档中的GG文件,其中1号为可以进入shipmode的文件,2号为不能进入shipmode的文件,谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,The only two requirements for Auto_Ship are AUTO_SHIP_EN = 1 and Auto Ship Time expires. There are however a long list of requirements to enter SLEEP from NORMAL mode including many safety alerts being clear. If you could provide a screenshot of the registers tab of BQStudio right before you stop communicating I can also check to see if any of these conditions may be preventing the device from entering SLEEP at all.
您好,已经在E2E英文论坛发贴,请关注该帖。
您好,Key things to be aware of are:
1- Make sure it is in shutdown mode and not communication can happen for Auto Ship Time. (if testing in BQStudio, make sure the scan button are OFF)
2- charger is not attached
3- make sure the working units have the same settings as the non-working parts.