This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54340输出电压与理论值有差异

我们在官网上设计电路时输入我们的输入电压,需求电流和环境温度,得到一个提供的稳压电路,我们按照官网给的电路图去配置,测试时发现实际值输出和理论值输出有差异,研读手册时,我把问题锁定在了这个电阻Rfbt,降低阻值发现电压会有相应的变化,但并非维持一个线性关系,最后输出到准确的理论值时这个电阻被降到了11.5K,和原来的53.6K差的还是挺大的,在24V-5V和24V-12V都有这样的规律,我们现在可以肯定的是电路的应用不会有错,各元器件都是官网提供的参数,希望得到大神的帮助,谢谢