This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76952: 电流和温度检测功能

Part Number: BQ76952


我目前在调试BQ76952时遇见一些问题,还请帮忙解答下,谢谢!

1 电流

1.1 电流采样有波动,1A测试时读取的电流为897~1009mA5A测试时读取的电流为4708~4820mA,请问这种情况该如何改善(该电流使用CC1计算,单位配置为1mA

1.2 CC1每250ms生成一次输出,该值输出的标志位是什么?

1.3 官网的demo中使用FULLSCAN作为电压、电流、温度等采样转换完成的标志,是否意味着该标志位每250msAFE置位?

1.4 FULLSCAN和ADSCAN区别是什么?如果只读取电芯电压,是否只需要判断ADSCAN标志位就行?

 

2 热敏电阻

2.1 在使用TS1测量温度时,将其配置为热敏电阻模式,18K上拉,报告原始ADC计数。在计算热敏电阻阻值时,上拉电阻是按照18K来计算的吗?是否能通过寄存器读出更准确的值?

2.2 REG18如何根据16AD值(DASTATUS5)计算出实际电压?