This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS55288: SW1對地短路

Part Number: TPS55288

1. IC工作說明及設定:

   線路需求 :VO:12V~24V,VL:12V(max100W)

   測試環境:VO輸入20V,VL負載机抽載8A

                    (** D5 by pass)

   寄存器設定: REF = 0x230

                         IOUT_LIMIT = 0xE2

                         VOUT_SR=0x30

                         VOUT_FS=0x03

                         CDC = 0xE7

                         MODE= 0xA4

2.問題描述:

  負載机設定8A,啟動抽載(ON)可正常輸出12V,10秒後關閉抽載(OFF)輸出降為0V,此狀況不定時發生,有時在抽載(ON)過程就發生異常。量測Q2 D-S腳短路原以為是Q2燒毀, 取下後發現Q2正常而是U3 SW1對地短路。以上問題求助各位大大,附上原理圖和Layout圖。

Schematic

Top Layout

Bot Layer

Inr Layer