This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV62585: 不明原因,芯片多次烧坏导致输出对地短路

Part Number: TLV62585

使用TLV62585DRLR作为5V转3.3V的应用,出现多次芯片烧坏;同一个板子上用这个芯片作为5V转1.8V却没出现过问题;请问:

1、TLV62585适用于占空比大于50%的应用吗?

2、板子上兼容了TLV62585PDRLR,NC引脚默认接了1.8V上拉是否会对此有影响?

3、现在看到的一个芯片现象是,输入输出阻抗菊正常,但是SW看起来没有正常工作,请问可能有什么原因导致的呢?