This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65219EVM-SKT: 在TPS65219_GUI上配置了LDO1为3.4V后,实际上测试到的结果为1.79V,想要知道如何配置才能达到3.4V

Part Number: TPS65219EVM-SKT
Other Parts Discussed in Thread: TPS65219

在TPS65219_GUI上配置了LDO1为3.4V后,实际上测试到的结果为1.79V,想要知道如何配置才能达到3.4V。

VBUCK1、VBUCK2、VBUCK3、VLDO1、VLDO2均输出3.4V,目前就VLDO1异常,能否帮忙看一下是什么地方没有配置好,谢谢

l  硬件跳线帽连接配置:

接口编号

连接方式

J1

VSYS - 5VUSB

J2

VSYS - BUCK1

VSYS - BUCK2

J3

VIN_BUCK3 - VSYS

J4

VIN_LDO1 - VSYS

J5

VIN_LDO2 - VSYS

J6

VIN_LDO34 - VSYS

J7

I2C_SELECT - MCU_3V3

J8

VSEL - GND

J9

MODE/STBY - GND

J10

MCU_3V3 - MODE/RESET

other

无连接

l  软件配置:

l  实际测量结果:

测试端口

设置电压

实际电压

结论

VBUCK1

3.4V

3.35V

正常

VBUCK2

3.4V

3.32V

正常

VBUCK3

3.4V

3.36V

正常

VLDO1

3.4V

1.79V

异常

VLDO2

3.4V

3.39V

正常