This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

采用BQ24610无法对聚合物锂电池充电问题

Other Parts Discussed in Thread: BQ24610, BQ24650, BQ24600

用BQ24610对聚合物锂电池进行充电,刚上电时有电压输出但闪了下就保护起来了,还查不出原因。急啊

如附图在TP75这点电压闪了下就没了。在有工作指示灯刚上电时也不亮

SCHEMATIC1 _ 01_Charger.pdf
  • 测一下VREF和REGN电压是否正常,确认太阳能电池板能输出相应功率。建议用MPPT控制的bq24650,是专门针对太阳能充电的。

  • 我这边也是遇到同样的问题, VREF和REGN在上电池前都是正常的, 所以波形和电压输出都正常, 但是上电池充电时,就进不了充电状态。 PH输出为1V左右, HIDRV输出也是1V左右。 电压输出为1V。 电流消耗为0. 重新插拔电源输入后, 所有状态又正常, 插入电池充电后又什么都没了, 电流消耗又是0。 我测试了BQ24600的DEMO板, 当电池插入后,会比较短的时间停止工作, 电流消耗为0, 后马上启动充电。 但是BQ24610就死在电流消耗为0的状态下, 启动不了充电, 感觉是内部程序不对。

  • 附加, 虽然电流消耗为0, 但是VREF是3.3V, REGN是1V左右。