This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM61480-Q1: 关于LM61480的PG lower threshold设置在FB电压的96.5%是否不合理?

Part Number: LM61480-Q1
Other Parts Discussed in Thread: LM61480

关于LM61480的PG lower threshold设置在FB电压的96.5%是否不合理?一般输出电压正常波动范围在95%~105%(Vo±5%),若在96.5%就进入VRESET_UV,RESET PIN被拉低,后级电源一般拿这个信号做EN信号,进而后级电源掉电,算是误操作行为。