Other Parts Discussed in Thread: LM61480


关于LM61480的PG lower threshold设置在FB电压的96.5%是否不合理?一般输出电压正常波动范围在95%~105%(Vo±5%),若在96.5%就进入VRESET_UV,RESET PIN被拉低,后级电源一般拿这个信号做EN信号,进而后级电源掉电,算是误操作行为。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.


关于LM61480的PG lower threshold设置在FB电压的96.5%是否不合理?一般输出电压正常波动范围在95%~105%(Vo±5%),若在96.5%就进入VRESET_UV,RESET PIN被拉低,后级电源一般拿这个信号做EN信号,进而后级电源掉电,算是误操作行为。
HI
你提到的基准不对。举例说,一般DD/DC反馈基准误差为1%,反馈电阻误差为1%,这样输出一般误差不到3%。设置5V输出,那么输出范围就是4.85~5.15V. 假设这个时候输出电压是4.95V, 而PG判定超出范围是10%,那么这个10%是4.95的10%, 而不是设置输出5V的10%。
HI
按照你的例子,输出电压上升,高于5.15* 110% 是PG可能反转, 高出114%必须反转。输出下降低于5.15*96.5%PG可能反转, 低于出92%必须反转。这里PGreset实际是个固定值,并非范围值。
HI
注意是高于5.15*114%必须反转, 低于5.15*92%必须反转。
rising and falling是指输入电压上升,和下降的过程。