This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5116: 负电源输出纹波大

Part Number: LM5116


本设计24V输入,-15.6输出,设计输出电流1.5A,设计纹波30mv.设计按照TI POWER DESIGN仿真得出的。设计见如下图片。

实际电源纹波测试,空载的时候纹波见下图(黄色,切换频率250k) 纹波VPP最大为56.7mv

0.5A电流负载的时候纹波见下图(黄色,切换频率250k),纹波VPP最大为78.3mv

1.2A电流负载的时候纹波见下图(黄色,切换频率250k) 纹波VPP最大为116mv

测试结果远远大于TI POWER DESIGN仿真结果,最大30mv VPP的结果,辛苦帮忙排查分析下。如何定位到问题点。谢谢。