This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS23751: TPS23751 设计输出电压12V 目前只有 7.44V

Part Number: TPS23751
Other Parts Discussed in Thread: PMP11254, TL431, TL432

链接:pan.baidu.com/.../1pb5RuzhsizhCSjpAfVojvQ 提取码:1234

原理图如附件!

目前没用使用PSE 供电

直接在整流桥前面接入和 50V直流电压;PD 空载的情况下测试,VB(10Pin): 5V; VC(12Pin): 6.67V。  输出电压6V左右。

输出接18欧姆 负载, 输出电压为:7.44V ; GATE(13Pin):250K。

请教下:1. 输出电压偏低是什么原因。

              2.空载电压比带负载电压低 是否正常。

              3.输出电压如何调整。