我们使用控制器TPS63681+6*CSD95490输出300A最大电流,250A平均电流应用时,概率出现CSD95490烧坏,烧坏后VIN和SW管脚短路。
当前针对CSD95490进行测试,发现其VIN to VSW最小值为-4.98V,最大值为14.7V。
其最大值是满足<20V要求的,但其最小值过于小,不知道是否会导致烧坏MOS管。
请问手册中这个VIN to VSW (10 ns)最小值应当为多少,才不至于损坏MOS管呢?


This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我们使用控制器TPS63681+6*CSD95490输出300A最大电流,250A平均电流应用时,概率出现CSD95490烧坏,烧坏后VIN和SW管脚短路。
当前针对CSD95490进行测试,发现其VIN to VSW最小值为-4.98V,最大值为14.7V。
其最大值是满足<20V要求的,但其最小值过于小,不知道是否会导致烧坏MOS管。
请问手册中这个VIN to VSW (10 ns)最小值应当为多少,才不至于损坏MOS管呢?


Hi
datasheet没有给出这个规格,但是-4.98V是肯定异常偏大的,甚至可能造成上面的异常。
将电路放上来看一下? 另外建议你重点确认一下layout(波形上的震荡,一般是layout不好造成的)
Hi
建议你确认一下SW脚的layout以及snubber电路。