This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CSD95490Q5MC: 多相电源MOS管烧坏问题,以及VDS最大值问题。

Part Number: CSD95490Q5MC

我们使用控制器TPS63681+6*CSD95490输出300A最大电流,250A平均电流应用时,概率出现CSD95490烧坏,烧坏后VIN和SW管脚短路。

当前针对CSD95490进行测试,发现其VIN to VSW最小值为-4.98V,最大值为14.7V。

其最大值是满足<20V要求的,但其最小值过于小,不知道是否会导致烧坏MOS管。

请问手册中这个VIN to VSW (10 ns)最小值应当为多少,才不至于损坏MOS管呢?