This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34Z100-R2: BQ34z100-R2在第一次充电结束后,FC置1,寄存器中Qmax Cell 0也更新了,Update Staus变成05,但是我等了17个小时,VOK没有变成0,还需要继续等吗?

Part Number: BQ34Z100-R2
Other Parts Discussed in Thread: GPCCHEM, , GPCRB

你好,我使用国轩高科一款磷酸铁锂电池,单节电池电压3.2V,容量15AH,我用12节电池串联进行电量计学习;

步骤一、我首先确认了电池化学ID,单节电池化学ID487, 12节电池化学ID 448或者445;

步骤二、电量计芯片重新烧录原始固件0100_2_02-bq34z100.bqz,

步骤三、更新电量计寄存器参数,选择化学ID,然后校准电压电流温度;

步骤四、按照手册说明进行放电静置,发送IT ENABLE,充满后FC=1,Update Status更新成05,Qmax Cell 0也更新了;

步骤五:等了17个小时,VOK标志位未清0;

我想知道原因,我能否继续进行下一步放电操作?还是说继续等待,或者重新开始电量计学习?

我在英文论坛也问过,他们就是推荐各种PDF,但是我真的各种PDF都看了,这个芯片我搞了两个月了,之前用的电池是无法从05更新到06,现在的问题是VOK无法清0;

我参数设置如下表格,我更改的寄存器参数已经用红色标明,Upstatus和Qmax Cell 0用黄色标明了;

寄存器参数.csv

x 出现错误。请重试或与管理员联系。