This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM22677: 两片LM22677按照Self Synchronization设计,两片工作状态不一致不稳定

Part Number: LM22677
Other Parts Discussed in Thread: LM25149, UCC29002

按照手册上的自同步设计,使用两片LM22677,原理图如下:

进行测试时,电子负载6A,会出现以下几种情况:

1、其中一片基本不工作,温度大概30℃,另外一片温度大概在105℃。不同的板卡不一致,有的是片1工作片2不工作,有的是片1不工作片2工作

2、有一块板卡,好像两片交替工作,其中一片温度到90℃,温度就下降,另外一片温度会上升

麻烦帮忙分析下问题,谢谢