Other Parts Discussed in Thread: LM25149, UCC29002
按照手册上的自同步设计,使用两片LM22677,原理图如下:
进行测试时,电子负载6A,会出现以下几种情况:
1、其中一片基本不工作,温度大概30℃,另外一片温度大概在105℃。不同的板卡不一致,有的是片1工作片2不工作,有的是片1不工作片2工作
2、有一块板卡,好像两片交替工作,其中一片温度到90℃,温度就下降,另外一片温度会上升
麻烦帮忙分析下问题,谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
需要用均流设计来实现。否者2个芯片的电流不一样会造成上述情况,甚至不稳定输出(其中一路保护)。
为什么不选择一个输出能力更大的芯片方案来实现呢? 很多外置MOS的电源芯片都是可以做到的。选上述不能均流的芯片很麻烦,除了2个电源芯片外,还需要均流芯片,而且还要保证均流效果好。 如果一定要并联输出,可以选择电流模式的控制芯片来做。
Hi
外置MOS的电源方案带载能力下降,首先要确认功率电感饱和电流足够,同时确认电流保护,最后是功率回路尽量小。
均流芯片可以看看UCC29002.
推荐芯片,能否说明一下详细规格(输入输出电流等)。 或者你可以借助官网选择:webench.ti.com/.../switching-regulator