This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24171: 电源管理论坛

Part Number: BQ24171

根据BQ24171的datasheet,对于可插拔的电池有相关的检测流程。详见规格书9.3.15章节。

bq24171 JEITA-Compliant Stand-Alone, Switched-Mode Li-Ion and Li-Polymer Battery Charger With Integrated MOSFETs and Power Path Selector datasheet (Rev. C) (ti.com)

我用这款IC搭建的电路给2串电池充电。发现充电开始阶段,在维持500ms左右的100mA充电电流后停止充电,停止充电的时间大概也为500ms。停止充电期间,state由H变成L。最后一阶阶调高充电电流。

具体参照下方的波形图。

黄色:电池pack电压

蓝色:充电IC的SW

红色:充电电流

绿色:充电IC的State

这是符合9.3.15里的流程的吗?125mA充电电流是flow里红框的部分?停止充电的500ms是

蓝框部分检测到电池已连接,开始正式充电的切换时间吗?