This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5176: LM5176 TEC设计资料咨询

Part Number: LM5176


大神们好!

       我看到:使用 LM5176  的 TEC 设计方案,不知道能否做到0.01℃控温精度。

       目前我需要控制 5V 2A TEC控制、9V 1A TEC控制、12V 5A  TEC控制。

       请问有没有对应的原理图,能否发给我参考参考。。。

谢谢!