This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CSD95490Q5MC: 多相电源MOS管烧坏,怀疑PWM信号超标引起,以及TPS53681的demo板也有同样问题。

Part Number: CSD95490Q5MC
Other Parts Discussed in Thread: TPS53681

你好,

我们使用控制器TPS63681+6*CSD95490输出300A最大电流,250A平均电流应用时,概率出现CSD95490烧坏,烧坏后VIN和SW管脚短路。

当前针对CSD95490进行测试,发现其PWM信号最小值为-0.9V。此项手册中的标准是最小值-0.3V。测试结果如下。

随后我们采购了TPS53681的demo板进行PWM信号的测试。测试点实际是在demo板的背面刮孔进行。使用的探头是TDP0500差分探头,一端接PWM信号,另一端接MOS管PGND。

测试结果最小值为-0.43V,同样超过其手册标注的-0.3V。

我们怀疑这个问题有一部分原因是CSD05490的此芯片的问题,麻烦你确认一下了,谢谢!