This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS768: TPS76801QD电特性与手册描述不符

Part Number: TPS768

工程师你好。
我在使用TPS76801QD时发现以下两个问题:
第一,当使能端的电压小于或等于1.3V时,元件可以正常工作;超过时则不可。这一数值和数据手册上的描述不符,低于high-level input enable voltage的最小值而高于low-level input enable voltage的最大值。


第二,据数据手册第三页的注释的说明,最小输入电压的大小为2.7V或典型输出值加一,以大者为准。可是使用时发现当使能端电压为低电平时,只要输入值大于设定的输出值,元件就能输出设定的值。


我希望可以得到这一现象的解释。感谢你的回答。

  • Hi

        1. 如你所说,按照参数表,EN>1.7V是芯片必须关闭,EN<0.9V芯片必须开启。所以你在芯片启动控制上的电平控制可以选择例如0V/3.3V之类,需要避免0.9~1.7V之类的电压控制。

        2. 作为LDO, 输入电压必须大于输出+Vdropmax, 而芯片最小输入电压是2.7V,  所以才说最小输入电压需要大于2.7V和Vo+1V。(1V是预估Vdropmax)