你好,
1.想了解为什么大多数恒流芯片反馈电压在0.2V左右,而恒压芯片一般电压在0.6V至1.25V左右?
2.恒流输出(反馈电压0.2V左右)能够改为恒压输出吗,规格书标定恒流的芯片改为用于恒压,会有什么风险和注意点呢?(环路参数调整?)
3.为什么芯片规格书一般0.2V是恒流芯片,0.8V是恒压芯片
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI
减小sense电阻功耗, 功耗是U^2/R, 显然小的基准电压sense电阻功耗会小很多。
而恒压就没有这个问题。恒压时分压电阻都很大,电流很小,功耗也会非常小。
Hi
两种控制完全不一样,恒压控制反馈是电压误差运放输出分压和三角波做duty控制。而恒流模式一般都是侦测电流,如TPS92691先采用放大器等很多电路后再做duty控制。不同的控制,没有理由将基准统一。电流基准几乎都是0.2V, 但电压基准就很多了,0.6V,0.8V,1.2V.
另外如你说说,抗干扰能力,1.2V显然比0.2V好很多,所以也就会导致恒流控制电路中复杂很多。