This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS92633-Q1: I(Quiescent)参数是在什么条件下测得的?

Part Number: TPS92633-Q1
PARAMETER TEST CONDITIONS MIN TYP MAX UNIT
I(Quiescent) Device standby ground current PWM = HIGH         1.5    2.5  mA

目前我配置IREF=100uA,所以I_SLS=100uA、ICTRL=1mA,此时芯片总功耗为1.94mA,

(测试条件VS=12V,EN=PWM1=PWM2=PWM3=12V)

从数值上看IQ应该是不用减去电流镜功耗的,

但是如果我将IREF引脚配置的电流增大,IQ也会跟着增大甚至突破2.5mA。

那么我有以下疑问:

1、IQ电流是否减去三个配置引脚的电流镜电流;

2、如果不需要减去,那么规格书中的参数是在什么外围下测得的?

3、如果需要减去,IQ会明显偏小,此时无法和规格书匹配。