This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34Z100-G1: 关于BQ34Z100的SOC跳变问题咨询

Part Number: BQ34Z100-G1
Other Parts Discussed in Thread: GPCCHEM

Hi, TI团队:

     现象1:我在BMS单板上进行直接调节改变总压后,静置一段时间后,可以观察到SOC有逐步的朝着电压变大或变小的方向进行持续SOC的+1或-1,直到最后SOC会稳定在某个值。在这过程中SOC是平滑的变化的(我的配置中有开启平滑功能)。

     现象2:当我直接把总压调到一个较低的电压值时(接近欠压值,但还是大于欠压值的),会观察到静置一段时间后,SOC会直接跳0,无中间的平滑过程了。

     问题:

     1、关于现象1,SOC的变化此时是根据OCV进行调节的吗?

     2、关于现象2,可以解释一下,为什么SOC不会平滑了,以及在什么情况下,SOC会直接跳0?

     3、在SOC变化之前都需要进行静置,我这边测试出来的时间大部分都是在几十分钟不到一小时,关于这个时间有具体的逻辑吗,以及在这过程中是否需要电流为0?(或小于某个值?)电压是否需要足够稳定?

     4、关于SOC的变化,除了正常的充放电变化外,还有什么情况下,SOC会进行变化?

  • 您好,请参考下面文档• RSOC 更新机制

    www.ti.com.cn/.../zhcaaf7.pdf

  • 您好,感谢您提供的文档。文档中是有描述可以通过开启平滑处理使得SOC不会跳变,但是我的配置中,已经开启了平滑处理, ,但是依然会出现直接跳变为0的情况 ,麻烦您讲解一下这个现象和逻辑。谢谢

  • 您好,您的CHEM ID是否配置并且完整学习,请将GPCCHEM report,log数据和.gg 文件发过来看一下。

  • 您好,应该是没有完整学习的,我是在BMS单板上进行调试测试的。我的疑惑点是,当我调节总压时,如果调后的总压不是接近欠压值的话,SOC是会逐渐减1减1的平滑下降(这里应该是我开启了SOC平滑配置的效果),但是当我将总压调节到比较低的一个值后,SOC平滑的功能似乎消失了,SOC会直接跳0值。这里应该是如何解释与理解呢,是34Z100中有针对低压时,SOC跳0的特殊处理吗?同样,当我将电压调到较高的值时(接近满充电压),SOC也会直接跳100。LOG日志链接:https://kdocs.cn/l/cfsyRQwS8ejD
    GG文件链接:kdocs.cn/.../camiiyl065lZ