Other Parts Discussed in Thread: GPCCHEM
Hi, TI团队:
现象1:我在BMS单板上进行直接调节改变总压后,静置一段时间后,可以观察到SOC有逐步的朝着电压变大或变小的方向进行持续SOC的+1或-1,直到最后SOC会稳定在某个值。在这过程中SOC是平滑的变化的(我的配置中有开启平滑功能)。
现象2:当我直接把总压调到一个较低的电压值时(接近欠压值,但还是大于欠压值的),会观察到静置一段时间后,SOC会直接跳0,无中间的平滑过程了。
问题:
1、关于现象1,SOC的变化此时是根据OCV进行调节的吗?
2、关于现象2,可以解释一下,为什么SOC不会平滑了,以及在什么情况下,SOC会直接跳0?
3、在SOC变化之前都需要进行静置,我这边测试出来的时间大部分都是在几十分钟不到一小时,关于这个时间有具体的逻辑吗,以及在这过程中是否需要电流为0?(或小于某个值?)电压是否需要足够稳定?
4、关于SOC的变化,除了正常的充放电变化外,还有什么情况下,SOC会进行变化?