This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65261: tps65261-1evm,对于VDIV引脚的处理

Part Number: TPS65261


各位设计师,你们好

我们最近使用了TPS65261电源芯片。在看开发板图纸时发现这个问题:

芯片手册中说明:VDIV引脚低于1.23V时,RESET引脚将会被拉低。

在开发板图纸中,VDIV引脚采用的电阻是146K和20K,输入电压为4.5V~18V。

此时,若输入电压为5V时,VDIV引脚电平应为:20/166*5=0.6V,

按照手册,此时复位引脚会被拉低,芯片无法工作。请问这里该如何理解?是手册描述有误吗?输入电压范围没有这么大?