This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76930: 在低温-40℃时,会触发硬件短路保护

Part Number: BQ76930


在低温-40℃,待机时,没接负载和充电,会触发硬件短路保护,但读到的电流是正常的,常温下不会出现这个现象

  • 感谢您对TI产品的关注!
    关于你的咨询,BQ76930 正常的工作温度范围就是-40~ 85℃.
    最低工作温度为-40度,温度达到最低温度时,注意温度的控制要精确,如果低于了-40度,可能就会导致工作不正常.
    另外,容易忽略的是比如,外围无源器件的设计,比如电容,晶振等,能否承受-40度的低温。
    如果电容失效了,对地就直接开路或短路了。
    有客户验证过-40度的低温下,这个芯片的放电是正常的。
    谢谢!

  • 外围元件都支持-40℃温度的,低温可以使用,在放电30A以下不会触发硬件短路保护,在放电超过30A以上时就会触发硬件短路保护,我的短路保护电流设置是100多A

  • 那你在-30℃和-35℃温度下,测量结果是什么情况。