This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7A57: 无法输出电压,以及耐电流有问题

Part Number: TPS7A57


使用该器件产生3.3V的电压,我现在的输入电压是3.7V,BIAS和EN引脚是和VIN 连接在一起的,这个时候3.3V就没有产生,我将输入电压给到5.6V,这个时候该器件就可以输出3.3V,然后我接上峰值电流有2.5A的负载,该器件的输出电压3.3V被拉低至3.1V