This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1、PMICA is TPS65941213;PMICB is TPS65941111
2、Scalable-PMICs-GUI version is 3.0.0
3、PB2 (SCL) and PB3 (SDA) linked to I2C1 of PMIC A using MSP-EXP432E401Y; PB2 (SCL) and PB3 (SDA) are pull-up to VCCA_3V3 using 10K ohm resistors
4、MSP-EXP432E401Y can connect to PMICA but cannot burn NVM configuration; As shown in the following picture;Unable to connect to Page0
5、What can I do to solve this problem:PMICA Unable to connect to Page0
Hi,
Please post your query in E2E English Forum as link below.
https://e2e.ti.com/
TI's product line experts will answer your question.