This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ4050: FCC无法通过完全放电更新,Max Error无法校准为2%,EDV0不跳变

Part Number: BQ4050


使用bq4050芯片对4s5p(4串5并)的磷酸铁锂电池组进行电量监测中出现学习与故障
在新的芯片中写入先前配置完毕并导出的gg.csv文件后,使用充至FC位并放到CUV位的方法并不能使BQ4050正确学习电池容量,同时放电到CUV电池仍还有1%电量显示
使用默认配置/未配置的bq4050芯片写入附件已经配置就绪的gg.csv文件即能复现
请求帮助:

1.为什么Max Error不更新,FCC容量不校准

2.为什么电池电量百分比截止到1%而不跳变

ceshi.gg.csv