The circuit above needs to be capable of delivering an output voltage of 5V and an output current of 10A when the input voltage is 12V.
However, the circuit is currently operating in a state where it shuts down the output when the load is at 0.3A, despite the input being 12V and the desired output being 5V."
Upon verification with the manual, resistors R2, R3, R4, R5, and R7 have been replaced with 0-ohm resistors. Consequently, with a load of 0.8 amperes, the power supply provides no output.
When the circuit is adjusted to have an input of 5V and an output of 3.3V, it can handle a load of 5A.
If I want to implement a circuit that has an input of 12 volts and provides an output of 5 volts with an output current of 10 amperes, how should I modify the circuit? Could you please help me with that?