现有6串50并的LED阵列需要驱动,单个LED最大电流40mA,VF=6V
50并之后的总电流为2A,
(1)想用TPS923655来驱动,LED阵列链接方式如下图所示,这样是否可行
(2)该芯片的电流限制可以到6.5A,这个意思是不是该芯片内部的MOS管可以承受6.5A以下的任意电流值?
(3)在驱动LED阵列的时候该芯片是不是恒压恒流输出,上图中二极管D之后的电流采样电阻是不是做恒流控制的
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好
1、可以这样设计,但是您的外围电路匹配。因为需要使IC能够满足足够大的输出功率。
2、TPS923655的电流限制功能允许您设置最大输出电流,以防止LED或其他负载过流。这里的“6.5A电流限制”是指该芯片在特定条件下(如合适的散热条件和输入电压范围内)可以承受的最大输出电流。
这并不意味着芯片内部的MOSFET可以承受6.5A以下的任意电流值。实际上,MOSFET的承受电流能力与其具体设计和工作条件有关。在TPS923655中,MOSFET的承受电流能力已经根据芯片的整体设计和应用需求进行了优化。
3、二极管D之后的电流采样电阻是用于监测输出电流的。这个电阻的阻值需要根据TPS923655的要求和LED阵列的实际需求来选择,以确保准确的电流采样和反馈。
您好,
3、实际情况您选择的模式不同,结果不同,您如果配置成恒压模式,理论上会输出功率会变小,输出电压不变,负载变大(并联数量减小,负载电阻变大),导致电流变小。反之恒流模式就不会变。理论上应该不会触发报警。建议您以测试情况为准。
4、对于TPS923655芯片,在分析其输出电流是否随负载电流变化而变化时,我们可以从以下几个方面进行考虑:
总结: