This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP5891-Q1: LP5891-Q1

Part Number: LP5891-Q1
Other Parts Discussed in Thread: LP5891

我有2個問題想請問你們2位。

 問題如下所示:

  1. 我們嘗試量測”LP5891”這顆ICPWM信號,所以我們將示波器接LINE0

LINE1CH1LINE0的波型,CH2LINE1的波型。

從示波器看到如下所示:

 

請問這是什麼樣信號的波形?

 

  1. 我們嘗試計算流過單顆LED的電流是否與設定的電流是否相同。

下圖是我們量測的架構圖,

我們量測TILED燈板的總輸入電流是705mA

TI的電路設計總共使用16掃瞄線

TI的電路LED總共使用768顆。

計算過程如下所示:

705mA/768=0.918mA

0.918mA*16=14.68mA

這與原先單一通道設定最大輸出電流20mA是不吻合的?

少了約6mA

暫存器設定如下所示: