Other Parts Discussed in Thread: TPS2375
最近做了一块POE供电模块,PD采用的是TI的TPS2375,电路图在附件中。降压电路部分用48V的稳压源测试过,是正常的,能够稳定输出12V电压。但是我将PD和转换模块组合在一起时,用万用表在P1处却检测不到48V电压。我在P1处并联一个小功率的48V用电设备。这时P1处又能量到48V电压,降压电路耶工作正常了。请问这是什么原因,我该做什么处理?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TPS2375
最近做了一块POE供电模块,PD采用的是TI的TPS2375,电路图在附件中。降压电路部分用48V的稳压源测试过,是正常的,能够稳定输出12V电压。但是我将PD和转换模块组合在一起时,用万用表在P1处却检测不到48V电压。我在P1处并联一个小功率的48V用电设备。这时P1处又能量到48V电压,降压电路耶工作正常了。请问这是什么原因,我该做什么处理?
楼主,你测试时是否使用的PSE供电?如果不是PSE供电,网线上是没有电压过来的,如果是PSE供电,看一下PD是否与PSE握手成功,PSE是否成功上电。
楼主,PSE和PD之间在正常握手供电之后,为了告诉PSE,PD仍然存在,PD需要有一个最小的维持电流,maintain power signature. 一个有效的PD端设备最小的维持电流一般是最少要有10mA。你描述的情况,看起来很像是没有足够的最小维持电流,导致PSE误认为PD设备已经移走,因此PSE才会断电。你现在测试一下PSE正常上电而PD后面不带载时,PD能拉多少电流,另外你的应用是有oring么?就是输入有PSE,也有适配器输入?能否把你oring的连接电路图发上来看看。