问:
bq2040推荐电路,是用bq2040的VOUT给24c01供电,但我实际测得VOUT引脚电压却只有150mv左右,这是正常现象?此时VCC为4V,ref也有输出为6V。
问:
bq2040只是对充电检测吗?适配器拔除,电池给负载供电,此时bq2040能检测电池电量吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
问:
bq2040推荐电路,是用bq2040的VOUT给24c01供电,但我实际测得VOUT引脚电压却只有150mv左右,这是正常现象?此时VCC为4V,ref也有输出为6V。
问:
bq2040只是对充电检测吗?适配器拔除,电池给负载供电,此时bq2040能检测电池电量吗?
插上电池后,VCC在EVM板内已经产生了,不需要外部的5V电源。
1,参考page 3 的表1,根据不同的电池类型以及串联数目,配置R4 R5 R11和Q1,这个非常重要,从而得到合适的VCC.
2,把EV2200与BQ2040 和EEPROm连接好,参考user guide里面的描述.
3.下载安装好对应的EV2200 Software for bq2040
http://www.ti.com.cn/tool/cn/EV2200?keyMatch=ev2200&tisearch=Search-CN-Everything
4,插入电池
5,按照user guide运行软件。
为了避免浪费资源,TI的大多数的软件都不再通过光盘等形式提供,改为在线下载的模式。以上谢谢!
注意表1 是针对的比6V还要高的电池应用中需要修改的电压调整电路配置,如果比6V低的则不需要开关管的调整。
同时TI建议使用该芯片的电池电压大于3V。谢谢!