This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

充电IC是如何判断采样电阻阻值的?

Other Parts Discussed in Thread: BQ24133, BQ40Z50

1、充电芯片,比如BQ24133,其采样电阻Rac和Rsr可以在某范围内变动,但10mΩ和20mΩ对应的电流差别为2倍,IC是怎么知道电阻是10mΩ还是20mΩ呢?

2、我初步认为是这样的,不知对否:默认Rsr为10mΩ,其实不过Rsr实际焊接多大,IC会一直认为为10mΩ,如果你想使用20mΩ电阻,那就需要把Viset也设置为原理的2倍,这样采样电流才不变,是这种“将错就错”的方式?

3、那么问题来了,为什么要使用20mΩ的电阻呢?是不是为了精度更高些,同时为了兼容更多阻值的采样电阻?

请专家们帮忙解答一下~

4、同样,对于BQ40z50多节电量计,也是同样的原理吧?

非常感谢!

  • IC不需要知道是20mΩ还是10mΩ,他只要保证取样电阻上的电压是一个固定值就可以,别的参数不变,你选择10mΩ的,假设电流是1A,取样电阻上的压降是10mV,你换成20mΩ的,电路还是保证取样电阻上的压降是10mV,充电电流就变成了0.5A。采用多大的取样电阻,是根据你需要的充电电流及Vset来计算的。

  • DAW 你好,

    我想了解下内部的机制,I=Vset/20/Rac,电流主要由Vset决定,这里Rac不知道,芯片是如何知道电流I的。所以我认为是IC默认Rac为10mΩ来计算的,实际焊接的阻值不是很精确的,所以实际充电电流才会有偏差。如果焊接了20mΩ,那么充电电流就变成了0.5倍,那就需要将错就错,将Vset设为原来的2倍。你认为呢?

  • 已经说了,无论你选择多大的Rac,Rac上的最大电压都是固定的,芯片不需要知道电流,芯片只要限制了Rac上的最大电压就OK了,我前面已经说了,你开始焊接10mΩ,压降是固定的,你换成20mΩ,压降还是那个值,那么流过这个电阻的压降自然就变成了原来的0.5倍。在设计的时候,需要多大的电流是我们设计的目的,VSET是已知条件,那么为了让这个电流流过Rac产生需要的电压Vset,就需要我们去计算及选择这个电阻Rac.

    如果你原来是10mΩ,流过的电流是A,你焊接20mΩ的电阻,还希望电流是A,那就像你说的,需要将Vset设置为原来的两倍。

  • Thank you very much!我把它与电量计搞混淆了。