This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
使用LM3478做将锂电池升压输出到12V的电路。参考WEBENCH给出的电路。只是输入电容和输出电容都是为2×10uF。调试时发现输出电压纹波很大,在1.2V左右。而且电路工作时,会将供电的锂电池电压拉低到3V以下(在3.9V到2.8V之间波动)。请问这种问题是什么原因导致的。谢谢!
附上电路的原理图: