找一个电流能在1-150uA或者0-100uA之间调节的,精度达到5nA的可调电流源。或者有不满足条件的类似的也可以推荐来看看
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好
TI的这个品类的芯片只有4款,其中adjustable current source是LM334,LM234,LM134这三款。
您可以看一下这个品类,点击器件型号可以进入芯片产品页,里面有datasheet等信息。
您好
2.5V是推荐的使用范围的最小值,我们建议您在推荐的电压范围内使用。
TI无法保证低于2.5V电压时的准确性。
至于电路如何设计,见数据手册 8 Application and Implementation,写的比较全面。
这里也有一个使用了REF200的参考设计,只用了里面的电流源,您也可以看一下。
我能否这样使用,上半部分结构是数据手册里给的参考方案,如图1。因为这个电流源是可以根据比例N来控制电流大小的,我把这个电流源接到电流镜的输入端口,由输出端口对我的一个大电流进行分流,剩余的部分给运放进行放大,运放的端口有2V的偏压。请您帮忙看看这样使用能不能行。

有没有使用电流镜的案例,在只使用电流镜时,显然底部3号端口的电压V3=V5+VBE+VCE+IR,手册中中给的应用图例3号端口用了一个理想电流源隔离,但在实际使用的时候这个理想电流源怎么做,实际怎么使用这个电流镜。我在5号端口有一个2V的Vin,这样如果直接在3号端口施加电压就需要精确计算电压的大小,并且电流镜不能动态调整不同大小的电流复制。3号4号端口如何配置能做到动态调整复制的电流大小?