This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24780S: BQ24780SRUYR不充电

Part Number: BQ24780S


你好,

     BQ24780SRUYR这款IC在设计调试阶段发现不充电,请帮忙协助分析一下不充电的原因,谢谢!

测试如下:

电池15.3V,充电电源20V

PIN4 25.5V

PIN5 3.3V

PIN6 2.8V

V_SYS 20V,说明前端2MOS管都导通了

PIN26 15.3VPIN2715.3V(示波器测试的),这里似乎应该是电荷泵开关,电感储能给电池充电,实际是直流(电池电压)

PIN18 15.3V

R4C15C16 15.3V(电池电压),R4右边接电池正极