This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS63060中的Ilim问题

Other Parts Discussed in Thread: TPS63060

看了slva535a.pdf文档中的关于TPS63060的计算过程,有点疑问:公式7(Imaxout=Ilim-ΔImax/2)中的Ilim值是多少?按照第10页A.4反推计算,Ilim=4A,请问TI技术人员:这个值是4A吗?(在datesheet中没有找到这个值,所以有疑问)

我现在设计一款输入电压范围是2.5V~4.2V,输出电压是3.8V,输出电流1A,滤波电感3.3uH,效率取0.8,K取0.2,Ilim取4A,按照计算得出数据如下:

BUCK模式 ΔImax 0.037 A
Isw_max 1.018 A
Imax_out 3.982 A
BOOST模式 ΔImax 0.150 A
Isw_max 1.975 A
Imax_out 2.066 A

请问TI技术工程师,表格的数据是否可以满足我的设计要求?