This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24780S: 不充电问题

Part Number: BQ24780S


你好

这款在设计调试阶段,发现不充电。

测试如下

电池15.3V,充电电源20V

PIN4 25.5V

PIN5 3.3V

PIN6 2.8V

V_SYS 20V,说明前端2MOS管都导通了

PIN230V(示波器),这样下管G开关没有脉冲打开

PIN24   6V

PIN26 15.3VPIN2715.3V(示波器测试的),这里似乎应该是电荷泵开关,电感储能给电池充电,实际是直流(等于电池电压)

PIN18 15.3V