![](/resized-image/__size/640x480/__key/communityserver-discussions-components-files/24/image004_2800_06_2D00_27_2D00_10_2D00_02_2D00_06_2900_.png)
你好
这款在设计调试阶段,发现不充电。
测试如下
电池15.3V,充电电源20V
PIN4 25.5V
PIN5 3.3V
PIN6 在2.8V
V_SYS 20V,说明前端2个MOS管都导通了
PIN23为0V(示波器),这样下管G开关没有脉冲打开
PIN24 6V
PIN26 15.3V,PIN27为15.3V(示波器测试的),这里似乎应该是电荷泵开关,电感储能给电池充电,实际是直流(等于电池电压)
PIN18 15.3V
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好
感谢您对TI产品的关注!为更加有效地解决您的问题,我们建议您将问题发布在E2E英文技术论坛上(https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum),将由资深的英文论坛工程师为您提供帮助。