Other Parts Discussed in Thread: LM76003
Hi,E2E
您好,请教两个问题,1 关于LM76003的17 pin(SYNC/MODE),当使用强制PWM模式时,可以通过10K电阻上拉到VCC pin上么,还是一定要直接接到VCC pin上
2 关于输出电感感值选型的问题,按照手册推荐,5V输出,500K开关频率,3.5A输出,感值是6.8uH,但是相同条件,WEBENCH的结果是10uH,所以按照哪个结果为准呀
以上,两个问题,麻烦帮忙解答一下,谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,E2E
您好,请教两个问题,1 关于LM76003的17 pin(SYNC/MODE),当使用强制PWM模式时,可以通过10K电阻上拉到VCC pin上么,还是一定要直接接到VCC pin上
2 关于输出电感感值选型的问题,按照手册推荐,5V输出,500K开关频率,3.5A输出,感值是6.8uH,但是相同条件,WEBENCH的结果是10uH,所以按照哪个结果为准呀
以上,两个问题,麻烦帮忙解答一下,谢谢
您好,
1:可选择直接接到VCC
2:这个建议仿真一下,应该不会有太大的影响,可以参考希下面链接的英文论坛专家的回复
WEBENCH的计算中,通常根据纹波电流(输出电流的百分比,通常为 30%)确定电感器的大小,如果您指定较小的输出电流,最终可能会得到比数据表中指定的更大的电感器。
您可以先仿真下,或者先按照webench推荐的值来先测试。