This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM76003-Q1: 关于LM76003的MODE pin和输出电感选型问题

Part Number: LM76003-Q1
Other Parts Discussed in Thread: LM76003

Hi,E2E

   您好,请教两个问题,1  关于LM76003的17 pin(SYNC/MODE),当使用强制PWM模式时,可以通过10K电阻上拉到VCC pin上么,还是一定要直接接到VCC pin上

                                       2 关于输出电感感值选型的问题,按照手册推荐,5V输出,500K开关频率,3.5A输出,感值是6.8uH,但是相同条件,WEBENCH的结果是10uH,所以按照哪个结果为准呀

    以上,两个问题,麻烦帮忙解答一下,谢谢