This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM76005: 输出有冲击能量,DC会损坏吗?

Part Number: LM76005

你好,我在使用LM76005设计成12V输出的应用(输入25~42V,输出电流2A,板子原理图已参考LM76005QEVM)。

目前12V输出的负载会有一个反向能量(如图,电压最大20V,电流最大10A),该能力是系统问题,无法消除。请帮忙确认下,该反向能力会对DC照成损害或者其他风险吗?谢谢。