This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3478的boost电路不能正常工作

Other Parts Discussed in Thread: LM3478

各位好,我按照LM3478的数据手册以及WEBENCH的设计分别做了一个输入为25——30V,输出100V,0.5A的板子,但是两块都不能用,两个都是boost升压电路,基本结构差不多。我给板子空载上电,从0开始加,加到3V以上时就会有电流,加大5V时电流就很大,有0.4A左右,在往上加电源就过流保护了。我发现FB端一直是低于1.26V,DR端一直是高导致MOS管一直打开,电流很大。断开DR和MOS管G级连接,直接在mos管上加一个350KHz,占空比为0.2的方波,mos能正常导通和关闭,输出电压也上去了,52V,提高输入电压和提高占空比能提高输出电压,在52V时带67欧的负载电压降至22V,电流0.4A。我在FB端直接给了一个三角波,峰峰值1.7V,FB能给出方波的波形。但是将芯片DR和mos的G连上后,输出电压就和输入电压几乎相等了。求各位能提供一些建议为什么会这样,怎么解决呢?附上原理图PCB和各点电位测量图。芯片是TI申请的。

想要解决的问题:

 1.为什么芯片DR和MOS的G连接后不能正常工作?

 2.为什么加大电压后mos一直导通,电流很大,输出不正常?

3.为什么我在FA/SD端看不到芯片工作的波形,但是直接给FB接信号源后DR能输出方波?

4.COMP的补偿怎么匹配?

第一次发帖求助,有什么不足之处还请大家多多包涵,请大家指出我的错误,在此先谢谢大家了。

LM3478的问题,求解决.docx
  • 亲;这说明两个问题:

    1)你可能没有仔细研究过这个电路。基于能量守恒,输出100V0.5A;输入5V时的输入电流为100X0.5A/5=10A。即你的5V电源至少需要输出10A才能维持这个电路正常工作(效率100%时)。实际上会再大些。这点需要特别注意。

    2)合闸瞬间实质是个过载启动过程,低压启动导致过流保护也是正常现象。如果可能;建议用高些的电压启动。首次通电;建议限流驱动。

  • 可是我是空载情况下测的,改变反馈电阻的比例仍然不能输出想要的电压,而且选择频率的引脚fa端并没有看到震荡的波形,而且在空载的时候输入电压一旦高于mos的开启电压之后mos一直导通,如果输入电压提高就会有很大的电流输出,就像我在附件中给的图片一样,在空载情况下4V输入情况下有0.4A的输入电流,而且这个芯片是可以在大于1.4V的输入电压下工作的,那么理论上空载情况下输出电压是能通过电感电容的充放电来达到一个100V的输出,只是被输入功率限制不能在100V带载,但是现在我的两块板子空载不能输出100V的电压,在附件里我也给出了对板子进行过独立的测试,断开芯片和mos的连接直接给mos波形,调节占空比是能够输出100V的,但是和芯片级连后就不能正常工作了。
  • 高压启动我也试过,25V输入,这已经是我设计的输入电压了,一节上去就被保护,电流有4-5A吧(应该是学生电源的过流限制在4-5A,输入电压马上就降向下来了,