This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RE:LM3150电流达不到10A问题

Other Parts Discussed in Thread: LM3150

我现在准备用LM3150搭一个输入24V,输出12V10A的电源。使用电感是3.3uH。高压侧MOS管使用的是CSD18533,现在电压输出有12V。我接上2欧电阻做负载测试时,电压下跌到3.3V,电流严重不够。请帮忙分析分析。

SCHEMATIC1 _ Socket20150226_2.pdf