我用的是TI公司提供uc3875拓扑原形。改为用ir2113的浮驱方式。
原来的模块输入电压是400VDC输入的。
现在模块的输入电压改为220VDC输入。
同样要求48V输出。
我也把管子从原来的ixtq22n50改为ixtq36n30。谐振电感从原来的10uH改为5.4uH。
原来电路可以到3000W,但是现在只能去到2100W左右,发热就很厉害了。看GD和DS的波形,基本判定没到软开关状态。
请问控制电路需要改元件吗?比如死区时间?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我用的是TI公司提供uc3875拓扑原形。改为用ir2113的浮驱方式。
原来的模块输入电压是400VDC输入的。
现在模块的输入电压改为220VDC输入。
同样要求48V输出。
我也把管子从原来的ixtq22n50改为ixtq36n30。谐振电感从原来的10uH改为5.4uH。
原来电路可以到3000W,但是现在只能去到2100W左右,发热就很厉害了。看GD和DS的波形,基本判定没到软开关状态。
请问控制电路需要改元件吗?比如死区时间?
从设计看,很多元件都已经换了,建议你参考移相全桥的ZVS实现条件重新计算下谐振电感的设计,因为ZVS的实现和谐振电感,工作电流和MOS的寄生电容都有关系。另外变压器的也需要重新设计,原边的工作电流都增加。