Other Parts Discussed in Thread: UC3875
我用的是TI公司提供uc3875拓扑原形。改为用ir2113的浮驱方式。
原来的模块输入电压是400VDC输入的。
现在模块的输入电压改为220VDC输入。
同样要求48V输出。
我也把管子从原来的ixtq22n50改为ixtq36n30。谐振电感从原来的10uH改为5.4uH。
原来电路可以到3000W,但是现在只能去到2100W左右,发热就很厉害了。看GD和DS的波形,基本判定没到软开关状态。
请问控制电路需要改元件吗?比如死区时间?