按照lm5050手册中的典型应用电路,搭了一下,想验证一下功能。电路如图,负载为1K电阻和led灯串联,OFF管腿接地,其他按照下图连接,左侧5V电源供电,芯片从OUT一侧取电,负载led被点亮,但测得GATE和IN管腿的电压也就是MOSFET的Vgs是-0.2V的电平,MOS管没有打开,而MOSFET的Vsd为0.5V左右,应该只有体二极管在导通,不知道问题出在哪里。后来换了12V的DC电源也是这样。如果MOSFET没有被打开,lm5050的作用就不能发挥,就不能检测到反向电流而关断MOSFET了,那这里的MOSFET就只能相当于一个二极管了,与二极管并联的电源冗余结构还有什么区别。想问问为什么lm5050没有正常工作。