This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS1HTC30-Q1: TPS1HTC30-Q1

Part Number: TPS1HTC30-Q1


Hi,

I'm testing this smart high-side switch.

This IC max current is 6A.

Vs pin = 24~26V

EN = 5V

ILIM = 24Kohm to GND.

Theoretically the current limit should be 4.16A

when I put the load on the Vout, setting the current over 4.16A.

this IC should hold the current 4.16A.

until temperature exceeding the permitted value

Overload and short to ground detection

BUT! 

Actually ,when the load current over 4.16A, TPS1HTC30-Q1 didn't hold the current

Instead, it quickly shorted out and the temperature rose to over 140 degrees Celsius.

what am i missing or wrong?